Part Number: PROCESSOR-SDK-AM335X
Tool/software: TI-RTOS
Hi there,
I am currently evaluating the use of Ti-Rtos on a am335x device (currently on a beaglebone black). At the moment the use-case i am working at is to discover/reset the network configuration of the device without physical access to the device. The only connection to the user is via network. Therefor the best solution would be a second pre-defined network configuration/IP-address on the network interface. I am wondering if that is possible in the current ndk version or if there is any other good solution for this case.
I am currently working with CCS 7.0.0.00043 on windows, SYS/BIOS V6.46.5.55, am335x PDK V1.0.7, NDK 2.25.1.11 and a beaglebone black rev c.
Thanks in Advance,
Jim