Hi,
I am working on speech recognition. My requirement is to be able to filter out unwanted background speech or music (usually low in amplitude) and consider only high amplitude voice data for recognition.
I am using a C5535 EZDSP board. I am using TI ESR library for speech recognition on the board. Although it works well, it does not have adaptive/active noise cancellation out of the box. I am planning to integrate it with a mic array and perform filtering of unwanted speech data. Is this possible on this platform?
Is there any add on board which can filter out unwanted speech, available as a separate board? or which can be integrated with c5535?
Also please suggest other TI boards if any support my requirement .
PS: By Noise cancellation, I mean filtering of unwanted sounds/speech/music.