We want to handle a video stream: 682*512, 50fps, raw data
If we using DM365 or DM6446:
1, How long does the davinci need when capture one frame and send to TV output?
1us or 10us or 1ms ?
We want to evaluate the video delay.
2, If pre-process have 60 frame progressive, how do the DM TV output module process it?
We need TV output the first field output the first frame's odd field,and the second filed output the second frame's even filed, and the third field output the third frams's odd field etc.
3, If the video source is 60fps , how do the TV output ?