Part Number: DM388
Hi,
I'm working on a an endoscope project which requires Full HD video capture and streaming using H.264 encoding @ 60fps, and the camera (Ominivision OV2740) is going to connect the CSI interface of DM388. In my application I need 2 independent display with two different video content simultaneously(smaller display is scaled version of Full HD content), and the display details are as shown below
Display 1 : 480x800, 24bit TFT LCD using parallel interface
Display 2 : 1980x1024, 24bit HDMI video for external display
My question! , is it possible to support dual display in DM388 with two different contents ? please help!