This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Engine closed hangs with MVL5.0



Hi,

I am using the MVL5.0 with DM6467 EVM. I am facing the issue with engine closed hangs when I try to link one of communication protocol library that I have. It is working fine with MVL4.0. I do not understand what causing this issue.

When I executes below command without using the MPEG2TS muxer library at that time it is working fine.,

a. CERuntime_init()

b. Engine_open()

c. Engine_close()

d. CERuntime_exit()

but when try to execute any of the APi of MPEG2TS muxer at that time it is creating issue.

 a. CERuntime_init()

    b. Engine_open()

    c. Stack_Open()

    d. Stack_Close()

    e. Engine_close()

    f. CERuntime_exit()

Stack library is developed in C++. In this case it hangs at Engine_close() giving message as,

     'terminate called without an active exception'

Thanks for help in advance. Any kind of suggestion or help will be appriciated.

Thanks,

Dilip Patel