Part Number: PROCESSOR-SDK-DRA7X
Tool/software: Linux
Hello,
In my case, the kmscube use drmModeSetPlane to post display buffer ,but the cube running too slow on psdk 3.02.00.03 , it post buffer to display 60fps.
The attached patch file are my change to kmscube orgin code(git://git.ti.com/glsdk/kmscube.git). It also need modify the bootargs "omapdrm.num_crtc=2" to "omapdrm.num_crtc=1" when use the patch .
But when i run the same kmscube code in glsdk , it can post buffer to display 700~fps.
Does anyone know why Kmscube use drmModeSetPlane to post running too slowly on PSDK ?
Thanks & Best Regards.
Sid
https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/791/setPlanetocube.7z