Part Number: TMS320C5535
Tool/software: Linux
Hello, everyone
I've been trying to customize the trigger phrase on the C5535 DSP card as the Reference Guide says but with no luck whatsoever. I'm completely new to Linux, so that's a problem. Regardless, I think I have followed the instructions on the guide to the letter but a few problems showed up. (Also I think it's important to say that I am using Linux on a bootable USB. I don't know if that has something to do with anything, just wanted to clarify that.)
On the subsection 5.3.3 the number 3 says "Execute the following command: $make LinuxDebugGnu", by this I assume I only have to write "make LinuxDebugGnu" for the symbol $ is already there. So I did that and I got the next message on the terminal:
I think it didn't worked because the Dist directory is not created as the next sentence says. No "bin" folder was created and the "lib" folder is empty as shown below.
Any suggestions? Or does someone know another (preferably easier or not involving Linux) to customize or change the trigger phrase on the DSP? I heard it might be possible in MatLab. Any comments?
I'd appreciate any advice.
- Osmar