Hello,
I'm currently using the Mcasp to drive a daisy chain of TDM micrphones that require both a data and frame sync clock. I'm using the receive clock and frame sync from the MCASP however, in order to have the microphones initialize correctly, I need to delay the start of the frame sync by at least 10ms or more from the recieve Clock. Currently the MCASP enables both clocks simultaneously and I was wondering what the best approach would be to delay the two.
I'm working off a modified Audioloop example provided in the PDK 1.0.5 software package located under:
pdk_k2g_1_0_5\packages\ti\addon\audk2g
Any tips would be appreciated. Thanks!