Tool/software: Linux
We are working on AM335x SOM which has wake-up and sleep mode features on Linux-4.4 kernel.
Also we came to know that, the wake-up can be done only with uart0, touch, GPIO0 bank.
But we need GPIO1 bank to wake-up the SOM.
Do you have any solution ? if not is it possible to share the firmware of GPIO0 bank.
So that we will do modifications to wake-up the SOM with GPIO1 bank.