Other Parts Discussed in Thread: OMAP3530
Has anyone ever used the display subsystem function where the dual 10-Bit video DAC can be placed in test mode (on OMAP3530)? Either 10-bit external random data, or 10-bit internal register values can be routed directly to the DAC, bypassing the video encoder. I am trying to take advantage of the this test mode to route some data and do general processing on the GPU -- the overall platform I am using to do this is the Beagleboard. I'm also wondering if there are any limitations on which internal registers can be used,and generally, the overall performance of the test mode.