hello all,
I hv been working on NDK 1.92, although it works well on DM648(my board) however it halts after some time for which i hv no reason. Now shifting to the newer version i.e NDK 2.0 I found that it works only when we use the board between two PC's (with 1G connection and using all the 8 wires of LAN cable), it doesn't work when the board(DM648) is connected to a LAN and PC (with 100MB connection or while using only 4 wires of ETH cable). So is there any setting in the code that needs to be changed so that NDK 2.0 work equally well when the board is connected on 100MB between the LAN and the PC. I am also unable to make the bootloader of the code using NDK 2.0
kindly help me in this regard
waiting for ur reply...
Regards
Ahmed