Part Number: PROCESSOR-SDK-AM335X
Hi,
I am using an SDK03.03 linux build.
I enabled the logo in the kernel config and can see it is correctly put on the screen.
I want to modify the logo.c file to read a GPIO and depending on a value load one or the other logo.
If I try to include
#include <linux/gpio.h>
and use:
gpio_get_value(67);
I get errors during kernel load
[ 0.997713] Unhandled fault: external abort on non-linefetch (0x1028) at 0xfa1ac134
and a lot of weired prints:
[ 0.997848] 7980: c02cca2c c02d0204 00000000 00000018 cf0479b4 cf0479a0 c0630070 c02cc9f8
[ 0.997856] 79a0: cf3a4800 00000018 cf0479d4 cf0479b8 c030aab8 c0630034 cf006800 cf3a4800
[ 0.997864] 79c0: cf3a0e00 00000720 cf047a24 cf0479d8 c0303288 c030aa30 cf3a7500 00000000
[ 0.997872] 79e0: cf047a0c cf0479f0 c0370f50 cf006800 cf3a4800 0000003c 00000000 cf006800
until it stops:
[ 0.998933] Kernel panic - not syncing: Attempted to kill init! exitcode=0x00
00000b
Is this because I am using function incorrectly?
Or is it because I cant use this yet because something is not initialised yet?
Kind regards,
Ugnius