This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA726: u-boot splash screen question

Part Number: DRA726


I have been following the instructions in sprac49.pdf but am not sure how to set the pll values for our display.

Unless I am mistaken I would just need to change a few values to match our 12 inch display and remove the part for controlling the backlight.

For us we just turn a GPIO on, there is no backlight control from the DRA726 beside that. The I2C port on the LCD display is only for the egalax touch screen.

Where would I look for the pll values to use?

void video_pll_conf(u32 lcd_type)
{
   uint32_t regval, temp;


   switch (lcd_type)
   {
       case LCD_TYPE_7_INCH:
          /* 7" LCD */
          divider = 10 + 1;
          multiplier = 410;
          div_h11_clkcfg = 16 + 1;
          break;
       case LCD_TYPE_10_INCH:
          /* 10" LCD */
          divider =     8 + 1;
          multiplier = 421;
          div_h11_clkcfg = 8 + 1;
          break;
       default:
          hang();
   }

Here are the definitions for the LCD, our display is LVDS, it has a device that converts for the TI video output to LVDS.

               panel-timing {
                        clock-frequency = <93688800>;
                        hactive = <1920>;
                        vactive = <720>;
                        hfront-porch = <115>;
                        hback-porch = <20>;
                        hsync-len = <5>;
                        vback-porch = <3>;
                        vfront-porch = <32>;
                        vsync-len = <3>;
                        hsync-active = <0>;
                        vsync-active = <0>;
                        de-active = <1>;
                        pixelclk-active = <1>;
                };

Michel Catudal

ACTIA Corp