Hi,
I have designed the custom board using AM3354. Boot media i had set and NAND.
i m using TH58NVG4S0HTAK0 nand device.
Please let me know can i boot from this nand.
PFA NAND datasheet - TH58NVG4S0HTAK0.pdf
Please help on this.
regards
Sujay A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have designed the custom board using AM3354. Boot media i had set and NAND.
i m using TH58NVG4S0HTAK0 nand device.
Please let me know can i boot from this nand.
PFA NAND datasheet - TH58NVG4S0HTAK0.pdf
Please help on this.
regards
Sujay A
Hi Biser,
Device ID of TH58NVG4S0HTAK0 matches with the mentioned ID in the TRM of AM3354, But wanted to make sure can it be used for Booting.
Nand (TH58NVG4S0HTAK0 ) details is as below
Capacity: 16 GBIT (2G x 8 BIT)
Organization:
x8
Memory cell array 4352 x 128K x 8 x 4
Register 4352 x 8
Page size 4352 bytes
Block size (256K x 16K) bytes
Modes
Read, Reset, Auto Page Program, Auto Block Erase, Status Read, Page Copy,
Multi Page Program, Multi Block Erase, Multi Page Copy, Multi Page Read
8 bit ECC for each 512Byte
Number of valid blocks
Min 8032 blocks
Max 8192 blocks
Please help on this.
Regards
Sujay A