Anybody knows which revision of the RMII protocol the OMAP L137 is at? Since Revision 1.2 (dating back from 1998), CRS_DV is suppose to toggle at the end of a packet to indicate deassertion of CRS :
http://www.national.com/appinfo/networks/files/rmii_1_2.pdf (page 6)
while looking at :
http://focus.ti.com/lit/ds/symlink/omap-l137.pdf (p.107)
I'm under the impression that CRS_DV remains asserted until final data is transferred. I see no toggling taking place at the end of a packet.
However, CRS_DV is only suppose to toggle while receiving and the diagram at p. 107 appears to related to both Transmission and reception.
Thanks.