Part Number: TCI6638K2K
Other Parts Discussed in Thread: DA8XX
Tool/software: Linux
Hi All,
We are trying to up the 10 Gig Ethernet interface , the block diagram as below
Control Lines are as below and they are connected as per white paper(SPRY268.pdf)
XFP Power down o/p ( goes high to low and low to high after power up )
- XFP Power Disable o/p ( LOW when communication else high)
- XFP TX Disable o/p (LOW)
- XFP interrupt, Module absent, module NR, module LOS are i/p
We are using processor sdk 4.0.0.4. and in device tree file keystone-k2hk-netcp.dtsi enabled xgbe_serdes and netcpx , the link-interface<11> which is MAC-to-MAC in the netcpx changed to link-interface<3> ( MAC-to-fiber)
We are getting interface eth4 and eth5 but link is not up
Thanks in advance
Regards
Gireesh