This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5728: GP EVM camera issue

Part Number: AM5728


Tool/software: Linux

Hi all,

i have two camera module here,one is included in the box with the EVM board ,and another is a new one which i bought recently and got today. The old one can't be detected by the EVM board,i use the console command shows in the below picture, i also try several times to make sure that  camera board is seated properly in the connector slot,so i thought it may be a hardware problem and bought the new camera module and try the same operation like the old one ,however,it can't be detected either.So is there some dts or dtsi files need to be edit or other operation need to be done before the camera module can be detected? I don't change any dts or dtsi file used. I am confused,the sdk i used is ti-processor-sdk-linux-am57xx-evm-03.03.00.04. 

I'm wondering if someone can provide more insight for me on this! Thanks in advance!

P.S. two camera's pics and the dts file setting are showing below(the top one is new and bottom one is old ):