This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MVL 5.0 uImage hangs while booting (DM6446 DVEVM)



Hello,

I'm trying to update to DVSDK 2_00_00_22 and MVL 5.0, using these packages:

  1. dvsdk_setuplinux_2_00_00_22.bin,
  2. mvl_5_0_0801921_demo_sys_setuplinux.bin,
  3. mvl_5_0_0_demo_lsp_setuplinux_02_00_00_140.bin.

The problem is that I can boot neither the pre-compiled kernel image (dvsdk_2_00_00_22/PSP_02_00_00_140/bin/dm6446/uImage-dm6446) nor self-built image.

The boot process just hangs after uncompressing the image:

===============

U-Boot 1.1.3 (Mar 15 2006 - 11:42:19)

U-Boot code: 81080000 -> 81097320  BSS: -> 810A0230
RAM Configuration:
Bank #0: 80000000 256 MB
MY AMD Flash: 16 MB
In:    serial
Out:   serial
Err:   serial
ARM Clock :- 283MZ
DDR Clock :- 189MZ
Hit any key to stop autoboot:  0
TFTP from server 106.109.9.132; our IP address is 106.109.8.224
Filename 'uImage'.
Load address: 0x80700000
Loading: #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         #####
done
Bytes transferred = 2018344 (1ecc28 hex)
## Booting image at 80700000 ...
   Image Name:   Linux-2.6.18_pro500-davinci_evm-
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2018280 Bytes =  1.9 MB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
OK

Starting kernel ...

Uncompressing Linux..................................................................................................................................... done, booting the kernel.

===============


The old kernel I have been using before boots perfectly:

===============

TFTP from server 106.109.9.132; our IP address is 106.109.8.224
Filename 'uImage'.
Load address: 0x80700000
Loading: #################################################################
         #################################################################
         #################################################################
         ################################################################
done
Bytes transferred = 1323024 (143010 hex)
## Booting image at 80700000 ...
   Image Name:   Linux-2.6.10_mvl402
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    1322960 Bytes =  1.3 MB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
OK

Starting kernel ...

Uncompressing Linux..................................................................................... done, booting the.Linux version 2.6.10_mvl402 (tim@106-109-9-132) (gcc version 3.4.3 (MontaVista 3.4.3-25.0.309

CPU: ARM926EJ-Sid(wb) [41069265] revision 5 (ARMv5TEJ)
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
Machine: DaVinci EVM
...

===============

 

Can the reason for this be the old U-Boot 1.1.3 version?

Thanks.

  • I use the same U-boot version ,but I can boot MVL5.0.however,my issue is the new kernel can not ping my server.Do you also boot via TFTP?

  • I just tried this on my DM6446 EVM; I was using the pre-built uImage-dm6446 file included in the dvsdk_2_00_00_22/PSP_02_00_00_140/bin/dm6446 directory.  I was able to boot fine via TFTP and was also able to ping my host from my EVM (log below)

    -----

    MontaVista(R) Linux(R) Professional Edition 5.0.0 (0801921)

    156.117.95.149 login: root
    Last login: Thu Jan  1 00:00:54 1970 on console
    Linux 156.117.95.149 2.6.18_pro500-davinci_evm-arm_v5t_le #1 PREEMPT Wed May 20 01:14:17 IST 2009 armv5tejl GNU/Linux

    Welcome to MontaVista(R) Linux(R) Professional Edition 5.0.0 (0801921).

    root@156.117.95.149:~# ping 156.117.95.15
    PING 156.117.95.15 (156.117.95.15) 56(84) bytes of data.
    64 bytes from 156.117.95.15: icmp_seq=1 ttl=64 time=0.951 ms
    64 bytes from 156.117.95.15: icmp_seq=2 ttl=64 time=0.614 ms
    64 bytes from 156.117.95.15: icmp_seq=3 ttl=64 time=0.602 ms
    64 bytes from 156.117.95.15: icmp_seq=4 ttl=64 time=0.630 ms
    64 bytes from 156.117.95.15: icmp_seq=5 ttl=64 time=0.584 ms
    64 bytes from 156.117.95.15: icmp_seq=6 ttl=64 time=0.686 ms
    64 bytes from 156.117.95.15: icmp_seq=7 ttl=64 time=0.663 ms
    64 bytes from 156.117.95.15: icmp_seq=8 ttl=64 time=0.677 ms
    64 bytes from 156.117.95.15: icmp_seq=9 ttl=64 time=0.512 ms
    64 bytes from 156.117.95.15: icmp_seq=10 ttl=64 time=0.449 ms
    64 bytes from 156.117.95.15: icmp_seq=11 ttl=64 time=0.662 ms
    64 bytes from 156.117.95.15: icmp_seq=12 ttl=64 time=0.672 ms
    64 bytes from 156.117.95.15: icmp_seq=13 ttl=64 time=0.682 ms
    64 bytes from 156.117.95.15: icmp_seq=14 ttl=64 time=0.614 ms
    64 bytes from 156.117.95.15: icmp_seq=15 ttl=64 time=0.655 ms
    64 bytes from 156.117.95.15: icmp_seq=16 ttl=64 time=0.668 ms
    64 bytes from 156.117.95.15: icmp_seq=17 ttl=64 time=0.561 ms
    64 bytes from 156.117.95.15: icmp_seq=18 ttl=64 time=0.559 ms
    64 bytes from 156.117.95.15: icmp_seq=19 ttl=64 time=0.546 ms
    64 bytes from 156.117.95.15: icmp_seq=20 ttl=64 time=0.659 ms
    64 bytes from 156.117.95.15: icmp_seq=21 ttl=64 time=0.723 ms
    64 bytes from 156.117.95.15: icmp_seq=22 ttl=64 time=0.445 ms
    64 bytes from 156.117.95.15: icmp_seq=23 ttl=64 time=0.500 ms
    64 bytes from 156.117.95.15: icmp_seq=24 ttl=64 time=0.593 ms
    64 bytes from 156.117.95.15: icmp_seq=25 ttl=64 time=0.497 ms
    64 bytes from 156.117.95.15: icmp_seq=26 ttl=64 time=0.516 ms
    64 bytes from 156.117.95.15: icmp_seq=27 ttl=64 time=0.599 ms
    64 bytes from 156.117.95.15: icmp_seq=28 ttl=64 time=0.621 ms
    64 bytes from 156.117.95.15: icmp_seq=29 ttl=64 time=0.589 ms
    64 bytes from 156.117.95.15: icmp_seq=30 ttl=64 time=0.497 ms
    64 bytes from 156.117.95.15: icmp_seq=31 ttl=64 time=0.666 ms
    64 bytes from 156.117.95.15: icmp_seq=32 ttl=64 time=0.558 ms
    64 bytes from 156.117.95.15: icmp_seq=33 ttl=64 time=0.634 ms
    64 bytes from 156.117.95.15: icmp_seq=34 ttl=64 time=0.538 ms
    64 bytes from 156.117.95.15: icmp_seq=35 ttl=64 time=0.651 ms
    64 bytes from 156.117.95.15: icmp_seq=36 ttl=64 time=0.594 ms
    64 bytes from 156.117.95.15: icmp_seq=37 ttl=64 time=0.665 ms

    --- 156.117.95.15 ping statistics ---
    37 packets transmitted, 37 received, 0% packet loss, time 35992ms
    rtt min/avg/max/mdev = 0.445/0.608/0.951/0.096 ms
    root@156.117.95.149:~#

  •  

    Thank you for the reply.

    I guess that the silence after "........done, booting the kernel." most likely can be caused by execution of wrong instructions. Something could be wrong with entry point or other memory access issues, or the image could have been corrupted somehow during or after uncompressing. What can I do to check these things? Do you have other ideas?

  • I have seen similar situations happen in the past when loading incompatible kernel or when kernel gets corrupt somehow.  Normally this is resolved by using a known good kernel such as the pre-built one included in the dvsdk (see PSP directory).

  • Yes, I'm trying to boot the original uImage-dm6446 from dvsdk_2_00_00_22/PSP_02_00_00_140/bin/dm6446, it should be ok. And the MVL 4 kernel from LSP 1.20 PSP_01_20_00_014/bin/dm6446/uImage-dm6446) boots well!

    I wonder what have changed in the boot process since MVL 4.

  • perhaps u-boot?  Try upgrading to u-boot 1.2.0 (that is what I am using).  Also, if you could post a log of your u-boot environment variables, that may help pin-point the issue.

  • Exactly!

    Thank you, Juan!

  • I am using u-boot version 1.3.4 with Montavista 5.0.24 and I have the same issue. It seems that the uImage when it gets unzipped and felocate to RAM has the first 4 bytes as 60 00 00 00, not sure what it is. I  am wondering if you have resolved this issue and how. Thanks Regards Claudio Spinelli

  • I simply updated u-boot to 1.2 and the problem gone, so I did not dig deeply in these things.