Other Parts Discussed in Thread: THS8200, THS7303
Hi all
I use DM365 + THS8200 , I want change output use VGA
I need to modify those parameters ??
thanks ~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Are you developing under CCS or Linux at the moment? If you are under CCS, we don't have existing examples at the moment.
I would suggest you to read the following to gain more understanding on the peripherals/devices you are using
http://www.ti.com/lit/gpn/ths8200
and
http://www.ti.com/litv/pdf/sprufg9c
HELLO ,I use th dvsdk 4.02 ,
my project is "dm365+th8200+ths7303" VGA output 1280x720p
I change the
davinci_platform.c ->davinci_enc_priv_setmode
and add the ths8200.c driver , i have already get 720p VGA video,
but i found the video clolor is wrong,my program is :
________________________________________________
dm365- >davinci_platform.c ->davinci_enc_priv_setmode
davinci_enc_set_720p(&mgr->current_mode);
davinci_enc_set_internal_hd(&mgr->current_mode);
ths8200_setval(THS8200_720P_60);
______________________________________________
davinci_platform.c ->davincidavinci_enc_set_720p
/* Reset video encoder module */
dispc_reg_out(VENC_VMOD, 0);
enableDigitalOutput(1);
dispc_reg_out(VENC_VDPRO, 0);
dispc_reg_out(VENC_VIDCTL, (VENC_VIDCTL_VCLKE | VENC_VIDCTL_VCLKP));
/* Setting DRGB Matrix registers back to default values */
dispc_reg_out(VENC_DRGBX0, 0x00000400);
dispc_reg_out(VENC_DRGBX1, 0x00000576);
dispc_reg_out(VENC_DRGBX2, 0x00000159);
dispc_reg_out(VENC_DRGBX3, 0x000002cb);
dispc_reg_out(VENC_DRGBX4, 0x000006ee);
/* Enable DCLOCK */
dispc_reg_out(VENC_DCLKCTL, VENC_DCLKCTL_DCKEC);
/* Set DCLOCK pattern */
dispc_reg_out(VENC_DCLKPTN0, 1);
dispc_reg_out(VENC_DCLKPTN1, 0);
dispc_reg_out(VENC_DCLKPTN2, 0);
dispc_reg_out(VENC_DCLKPTN3, 0);
dispc_reg_out(VENC_DCLKPTN0A, 2);
dispc_reg_out(VENC_DCLKPTN1A, 0);
dispc_reg_out(VENC_DCLKPTN2A, 0);
dispc_reg_out(VENC_DCLKPTN3A, 0);
dispc_reg_out(VENC_DCLKHS, 0);
dispc_reg_out(VENC_DCLKHSA, 1);
dispc_reg_out(VENC_DCLKHR, 0);
dispc_reg_out(VENC_DCLKVS, 0);
dispc_reg_out(VENC_DCLKVR, 0);
/* Set brightness start position and pulse width to zero */
dispc_reg_out(VENC_BRTS, 0);
dispc_reg_out(VENC_BRTW, 0);
/* Set LCD AC toggle interval and horizontal position to zero */
dispc_reg_out(VENC_ACCTL, 0);
/* Set PWM period and width to zero */
dispc_reg_out(VENC_PWMP, 0);
dispc_reg_out(VENC_PWMW, 0);
dispc_reg_out(VENC_CVBS, 0);
dispc_reg_out(VENC_CMPNT, 0);
/* turning on horizontal and vertical syncs */
dispc_reg_out(VENC_SYNCCTL, (VENC_SYNCCTL_SYEV | VENC_SYNCCTL_SYEH));
dispc_reg_out(VENC_OSDCLK0, 0);
dispc_reg_out(VENC_OSDCLK1, 1);
dispc_reg_out(VENC_OSDHADV, 0);
// __raw_writel(0xa, IO_ADDRESS(SYS_VPSS_CLKCTL));
if (cpu_is_davinci_dm355()) {
dispc_reg_out(VENC_CLKCTL, 0x11);
osd_write_left_margin(mode_info->left_margin);
osd_write_upper_margin(mode_info->upper_margin);
davinci_cfg_reg(DM355_VOUT_FIELD_G70);
davinci_cfg_reg(DM355_VOUT_COUTL_EN);
davinci_cfg_reg(DM355_VOUT_COUTH_EN);
}else if (cpu_is_davinci_dm365()) {
osd_write_left_margin(mode_info->left_margin);
osd_write_upper_margin(mode_info->upper_margin);
/* DM365 pinmux */
dispc_reg_out(VENC_CLKCTL, 0x10);
davinci_cfg_reg(DM365_VOUT_FIELD_G81);
davinci_cfg_reg(DM365_VOUT_COUTL_EN);
davinci_cfg_reg(DM365_VOUT_COUTH_EN);
/* Set VIDCTL to select VCLKE = 1,
VCLKZ =0, SYDIR = 0 (set o/p), DOMD = 0 */
dispc_reg_merge(VENC_VIDCTL, 1 << VENC_VIDCTL_VCLKE_SHIFT,
VENC_VIDCTL_VCLKE);
dispc_reg_merge(VENC_VIDCTL, 0 << VENC_VIDCTL_VCLKZ_SHIFT,
VENC_VIDCTL_VCLKZ);
dispc_reg_merge(VENC_VIDCTL, 0 << VENC_VIDCTL_SYDIR_SHIFT,
VENC_VIDCTL_SYDIR);
dispc_reg_merge(VENC_VIDCTL, 0 << VENC_VIDCTL_YCDIR_SHIFT,
VENC_VIDCTL_YCDIR);
}else {
osd_write_left_margin(mode_info->left_margin);
osd_write_upper_margin(mode_info->upper_margin);
davinci_cfg_reg(DM644X_LOEEN);
davinci_cfg_reg(DM644X_GPIO3);
}
/* Set VENC for non-standard timing */
davinci_enc_set_display_timing(mode_info);
dispc_reg_out(VENC_HSDLY, 0);
dispc_reg_out(VENC_VSDLY, 0);
dispc_reg_out(VENC_YCCCTL, 0X0);
dispc_reg_out(VENC_VSTARTA, 0);
/* Enable all VENC, non-standard timing mode, master timing, HD,
progressive
*/
if (cpu_is_davinci_dm355()) {
dispc_reg_out(VENC_VMOD, (VENC_VMOD_VENC | VENC_VMOD_VMD));
} else {
dispc_reg_out(VENC_VMOD,
(VENC_VMOD_VENC | VENC_VMOD_VMD));
}
dispc_reg_out(VENC_LCDOUT, 0);
________________________________________-
th8200.c
int ths8200_setval(enum ths8200_modes mode)
{
int err = 0, disable = 0;
if (ths8200_client == NULL)
return 0;
switch (mode) {
case THS8200_720P_60:
printk("ths8200 set THS8200_720P_60\n ");
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CHIP_CTL, 0x01);//WR_REG,THS8200,0x01,0x03,0x01 // chip_ctl frequency range=high
//YCbR to RGB
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSC_R11, 0x81);//WR_REG,THS8200,0x01,0x04,0x81 // csc_ric1
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSC_R12, 0xD5);//WR_REG,THS8200,0x01,0x05,0xD5 // csc_rfc1
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSC_R21, 0x00);//WR_REG,THS8200,0x01,0x06,0x00 // csc_ric2
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSC_R22, 0x00);//WR_REG,THS8200,0x01,0x07,0x00 // csc_rfc2
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSC_R31, 0x06);//WR_REG,THS8200,0x01,0x08,0x06 // csc_ric3
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSC_R32, 0x29);//WR_REG,THS8200,0x01,0x09,0x29 // csc_rfc3
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSC_G11, 0x04);//WR_REG,THS8200,0x01,0x0A,0x04 // csc_gic1
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSC_G12, 0x00);//WR_REG,THS8200,0x01,0x0B,0x00 // csc_gfc1
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSC_G21, 0x04);//WR_REG,THS8200,0x01,0x0C,0x04 // csc_gic2
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSC_G22, 0x00);//WR_REG,THS8200,0x01,0x0D,0x00 // csc_gfc2
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSC_G31, 0x04);//WR_REG,THS8200,0x01,0x0E,0x04 // csc_gic3
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSC_G32, 0x00);//WR_REG,THS8200,0x01,0x0F,0x00 // csc_gfc3
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSC_B11, 0x80);//WR_REG,THS8200,0x01,0x10,0x80 // csc_bic1
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSC_B12, 0xBB);//WR_REG,THS8200,0x01,0x11,0xBB // csc_bfc1
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSC_B21, 0x07);//WR_REG,THS8200,0x01,0x12,0x07 // csc_bic2
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSC_B22, 0x42);//WR_REG,THS8200,0x01,0x13,0x42 // csc_bfc2
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSC_B31, 0x00);//WR_REG,THS8200,0x01,0x14,0x00 // csc_bic3
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSC_B32, 0x00);//WR_REG,THS8200,0x01,0x15,0x00 // csc_bfc3
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSC_OFFS1, 0x14);//WR_REG,THS8200,0x01,0x16,0x14 // csc_offset1
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSC_OFFS12, 0xAE);//WR_REG,THS8200,0x01,0x17,0xAE // csc_offset12
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSC_OFFS23, 0x8B);//WR_REG,THS8200,0x01,0x18,0x8B // csc_offset23
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSC_OFFS3, 0x15);//WR_REG,THS8200,0x01,0x19,0x15 // csc_offset3
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DATA_CNTL, 0x13);//WR_REG,THS8200,0x01,0x1C,0x53 // dman_cntl 20bit 422
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_Y_SYNC1_LSB, 0x00);//WR_REG,THS8200,0x01,0x1D,0x00 // dtg_y_sync1
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_Y_SYNC2_LSB, 0x00);//WR_REG,THS8200,0x01,0x1E,0x00 // dtg_y_sync2
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_Y_SYNC3_LSB, 0x00);//WR_REG,THS8200,0x01,0x1F,0x00 // dtg_y_sync3
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_CBCR_SYNC1_LSB, 0x00);//WR_REG,THS8200,0x01,0x20,0x00 // dtg_cbcr_sync1
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_CBCR_SYNC2_LSB, 0x00);//WR_REG,THS8200,0x01,0x21,0x00 // dtg_cbcr_sync2
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_CBCR_SYNC3_LSB, 0x00);//WR_REG,THS8200,0x01,0x22,0x00 // dtg_cbcr_sync3
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_Y_SYNC_MSB, 0x2A);//WR_REG,THS8200,0x01,0x23,0x2A // dtg_y_sync_upper
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_CBCR_SYNC_MSB, 0x2A);//WR_REG,THS8200,0x01,0x24,0x2A // dtg_cbcr_sync_upper
i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_SPEC_A, 0x28);//WR_REG,THS8200,0x01,0x25,0x28 // dtg_spec_a
i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_SPEC_B, 0x6E);//WR_REG,THS8200,0x01,0x26,0x6E // dtg_spec_b
i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_SPEC_C, 0x28);//WR_REG,THS8200,0x01,0x27,0x28 // dtg_spec_c
i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_SPEC_D_LSB, 0x04);//WR_REG,THS8200,0x01,0x28,0x04 // dtg_spec_d
i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_SPEC_D1, 0x00);//WR_REG,THS8200,0x01,0x29,0x00 // dtg_spec_d1
i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_SPEC_E_LSB, 0x04);//WR_REG,THS8200,0x01,0x2A,0x04 // dtg_spec_e
i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_SPEC_DEH_MSB, 0xC0);//WR_REG,THS8200,0x01,0x2B,0xC0 // dtg_spec_h_msb
i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_SPEC_H_LSB, 0x00);//WR_REG,THS8200,0x01,0x2C,0x00 // dtg_spec_h_lsb
i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_SPEC_I_MSB, 0x00);//WR_REG,THS8200,0x01,0x2D,0x00 // dtg_spec_i_msb
i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_SPEC_I_LSB, 0x00);//WR_REG,THS8200,0x01,0x2E,0x00 // dtg_spec_i_lsb
i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_SPEC_K_LSB, 0x6E);//WR_REG,THS8200,0x01,0x2F,0x6E // dtg_spec_k_lsb
i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_SPEC_K_MSB, 0x00);//WR_REG,THS8200,0x01,0x30,0x00 // dtg_spec_k_msb
i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_SPEC_K1, 0x00);// WR_REG,THS8200,0x01,0x31,0x00 // dtg_spec_k1
i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_SPEC_G_LSB, 0x00);// WR_REG,THS8200,0x01,0x32,0x00 // dtg_speg_g_lsb
i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_SPEC_G_MSB, 0x00);// WR_REG,THS8200,0x01,0x33,0x00 // dtg_speg_g_msb
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_TOT_PIXELS_MSB, 0x06);//WR_REG,THS8200,0x01,0x34,0x03 // dtg_total_pixel_msb adjust for various graphics formats
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_TOT_PIXELS_LSB, 0x72);//WR_REG,THS8200,0x01,0x35,0x5A // dtg_total_pixel_lsb
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_FLD_FLIP_LINECNT_MSB, 0x080);//WR_REG,THS8200,0x01,0x36,0x80 // dtg_linecnt_msb
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_LINECNT_LSB, 0x01);//WR_REG,THS8200,0x01,0x37,0x01 // dtg_linecnt_lsb
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_MODE, 0x87);//WR_REG,THS8200,0x01,0x38,0x87 // dtg_mode VESA Slave
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_FRAME_FIELD_SZ_MSB, 0x27);//WR_REG,THS8200,0x01,0x39,0x27 // dtg_frame_field_msb adjust for various graphics formats
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_FRAME_SZ_LSB, 0xEE);//WR_REG,THS8200,0x01,0x3A,0x0D // dtg_frame_size_lsb
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_FIELD_SZ_LSB, 0xFF);//WR_REG,THS8200,0x01,0x3B,0xFF // dtg_field_size_lsb
//CSM setup to map YCbCr to FS RGB
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSM_CLIP_GY_LOW, 0x40);//WR_REG,THS8200,0x01,0x41,0x40 // csm_clip_gy_low
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSM_CLIP_BCB_LOW, 0x40);//WR_REG,THS8200,0x01,0x42,0x40 // csm_clip_bcb_low
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSM_CLIP_RCR_LOW, 0x40);//WR_REG,THS8200,0x01,0x43,0x40 // csm_clip_rcr_low
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSM_CLIP_GY_HIGH, 0x53);//WR_REG,THS8200,0x01,0x44,0x53 // csm_clip_gy_high
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSM_CLIP_BCB_HIGH, 0x3F);//WR_REG,THS8200,0x01,0x45,0x3F // csm_clip_bcb_high
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSM_CLIP_RCR_HIGH, 0x3F);//WR_REG,THS8200,0x01,0x46,0x3F // csm_clip_rcr_high
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSM_SHIFT_GY, 0x40);//WR_REG,THS8200,0x01,0x47,0x40 // csm_shift_gy
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSM_SHIFT_BCB, 0x40);//WR_REG,THS8200,0x01,0x48,0x40 // csm_shift_bcb
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSM_SHIFT_RCR, 0x40);//WR_REG,THS8200,0x01,0x49,0x40 // csm_shift_rcr
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSM_GY_CNTL_MULT_MSB, 0xFC);//WR_REG,THS8200,0x01,0x4A,0xFC // csm_mult_gy_msb
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSM_MULT_BCB_RCR_MSB, 0x44);//WR_REG,THS8200,0x01,0x4B,0x44 // csm_mult_bcb_rcr_msb
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSM_MULT_GY_LSB, 0xAC);//WR_REG,THS8200,0x01,0x4C,0xAC // csm_mult_gy_lsb
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSM_MULT_BCB_LSB, 0xAC);//WR_REG,THS8200,0x01,0x4D,0xAC // csm_mult_bcb_lsb
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSM_MULT_RCR_LSB, 0xAC);//WR_REG,THS8200,0x01,0x4E,0xAC // csm_mult_rcr_lsb
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CSM_MULT_RCR_BCB_CNTL, 0xFF);//WR_REG,THS8200,0x01,0x4F,0xFF // csm_mode
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG2_HLENGTH_LSB, 0x28);//WR_REG,THS8200,0x01,0x70,0x40 // dtg_hlength_lsb adjust HSOUT width for various formats
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG2_HLENGTH_LSB_HDLY_MSB, 0x01);//WR_REG,THS8200,0x01,0x71,0x03 // dtg_hdly_msb
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG2_HLENGTH_HDLY_LSB, 0x04);//WR_REG,THS8200,0x01,0x72,0x31 // dtg_hdly_lsb
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG2_VLENGTH1_LSB, 0x05);//WR_REG,THS8200,0x01,0x73,0x07 // dtg_vlength_lsb adjust VSOUT width for various formats
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG2_VLENGTH1_MSB_VDLY1_MSB, 0x02);//WR_REG,THS8200,0x01,0x74,0x00 // dtg_vdly_msb
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG2_VDLY1_LSB, 0xED);//WR_REG,THS8200,0x01,0x75,0x07 // dtg_vdly_lsb
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG2_VLENGTH2_LSB, 0x00);//WR_REG,THS8200,0x01,0x76,0x00 // dtg_vlength2_lsb
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG2_VLENGTH2_MSB_VDLY2_MSB, 0x07);//WR_REG,THS8200,0x01,0x77,0xC7 // dtg_vdly2_msb
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG2_VDLY2_LSB, 0xFF);//WR_REG,THS8200,0x01,0x78,0xFF // dtg_vdly2_lsb
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG2_HS_IN_DLY_MSB, 0x00);//WR_REG,THS8200,0x01,0x79,0x00 // dtg_hs_in_dly_msb adjust for horizontal alignment
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG2_HS_IN_DLY_LSB, 0x0A);//WR_REG,THS8200,0x01,0x7A,0x0F // dtg_hs_in_dly_lsb
// err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG2_HS_IN_DLY_MSB, 0x00);//WR_REG,THS8200,0x01,0x79,0x00 // dtg_hs_in_dly_msb adjust for horizontal alignment
// err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG2_HS_IN_DLY_LSB, 0x32);//WR_REG,THS8200,0x01,0x7A,0x0F // dtg_hs_in_dly_lsb
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG2_VS_IN_DLY_MSB, 0x00);//WR_REG,THS8200,0x01,0x7B,0x00 // dtg_vs_in_dly_msb adjust for vertical alignment
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG2_VS_IN_DLY_LSB, 0x00);//WR_REG,THS8200,0x01,0x7C,0x00 // dtg_vs_in_dly_lsb
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG2_CNTL, 0x5B);//WR_REG,THS8200,0x01,0x82,0x5B // pol_cntl HS/VSin ++, HS/VSout++, FID -
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CGMS_CNTL_HEADER, 0x00);//WR_REG,THS8200,0x01,0x83,0x00
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CGMS_PAYLOAD_MSB, 0x00);//WR_REG,THS8200,0x01,0x84,0x00
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CGMS_PAYLOAD_LSB, 0x00);//WR_REG,THS8200,0x01,0x85,0x00
err = i2c_smbus_write_byte_data(ths8200_client, THS8200_CHIP_CTL, 0x00);
mdelay(50);
err = i2c_smbus_write_byte_data(ths8200_client, THS8200_CHIP_CTL, 0x01);
break;
default:
/* disable all channels */
printk("ths8200_colorbar \n");
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CHIP_CTL, 0x23);
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_MODE, 0x87);//WR_REG,THS8200,0x01,0x38,0x86 // dtg_mode VESA master
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG2_CNTL, 0x5B);//WR_REG,THS8200,0x01,0x82,0x5B // pol_cntl HS/VSin ++, HS/VSout++, FID -
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_VESA_CBAR_SIZE, 0x80);
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_SPEC_DEH_MSB, 0x00);
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_DTG1_SPEC_E_LSB, 0xC0);
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CHIP_CTL, 0x22);
mdelay(50);
err |=i2c_smbus_write_byte_data(ths8200_client, THS8200_CHIP_CTL, 0x23);
disable = 1;
break;
}
if (err)
{
printk("reset th8200 error!\n");
return err;
}
return err;
}
i don't know why the color is wrong? please help me .