This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCI6630K2L: Questions about discrepancies in TCI6630K2L datasheet and other docs

Part Number: TCI6630K2L

Hi All!

We are developing custom board with TCI6630K2L SoC and found some discrepancies in datasheet (www.ti.com/.../tci6630k2l.pdf) and other docs:

1. VDDCMON in Table 6-3 is connected to CVDDS (0.98V) and in http://www.ti.com/lit/pdf/sprac02 it is connected to CVDD (1V). Which one is right?

2. In Table 11-1 and Table 6-3 CVDD1 is 0.95V. In Table 10.2 CVDD1 is between 0.952V and 1.047V. Which one is right?

3. In Figures 6-3, 6-4, 6-5 and 6-6:

    - pin K8  - AVDDA1

    - pin J21 - AVDDA5

    - pin J17 - AVDDA4

    - pin J11 - AVDDA2

    - pin J14 - AVDDA3

    But in Tables 6-3 and 6-5:

    - pin K8  - AVDDA6

    - pin J21 - AVDDA10

    - pin J17 - AVDDA9

    - pin J11 - AVDDA8

    - pin J14 - AVDDA7

    Which one is right?

4. In Figure 6-6 VPH (3.3V) is at pin V8. In Tables 6-3, 6-4 and 6-5 pin V8 is at VP (0.85V). Which one is right?

5. Pins R13, R15, R17, R19 and R21 are not listed in Tables 6-3 and 6-4. Can we trust other tables regarding these pins?

Best Regards,

Yurii