Part Number: AM5728
Tool/software: Linux
Hello,
I want to use gstreamer to encode a video file,and here is my code:
#include <gst/gst.h>
int main(int argc, char *argv[])
{
GstElement *pipeline, *src, *video_parse, *myvpe, *enc, *sink, *capsfilter1;
GstCaps *caps1;
GstBus *bus;
GstMessage *msg;
GstStateChangeReturn ret;
gst_init(&argc, &argv);
pipeline = gst_pipeline_new("videoencoder");
src = gst_element_factory_make("filesrc", "src");
video_parse = gst_element_factory_make("videoparse", "video_parse");
myvpe = gst_element_factory_make("videoconvert", "myvpe");
capsfilter1 = gst_element_factory_make("capsfilter", "capsfilter1");
enc = gst_element_factory_make("ducatih264enc", "enc");
sink = gst_element_factory_make("filesink", "sink");
if (!pipeline || !src || !video_parse || !myvpe || !capsfilter1 || !enc || !sink)
{
g_printerr("One element could not be created.Exiting.\n");
return -1;
}
g_object_set(G_OBJECT(src), "location", "/mnt/akiyo_qcif.yuv", NULL);
g_object_set(G_OBJECT(video_parse), "width", "176", NULL);
g_object_set(G_OBJECT(video_parse), "height", "144", NULL);
g_object_set(G_OBJECT(video_parse), "format", 2, NULL);
g_object_set(G_OBJECT(video_parse), "framerate", 25,1, NULL);
caps1 = gst_caps_new_simple("video/x-raw",
"format", G_TYPE_STRING, "NV12",
"width", G_TYPE_INT, 176,
"height", G_TYPE_INT, 144,
"framerate", GST_TYPE_FRACTION, 25, 1,
NULL);
g_object_set(G_OBJECT(capsfilter1), "caps", caps1, NULL);
gst_object_unref(caps1);
g_object_set(G_OBJECT(sink), "location", "/mnt/b2b.h264", NULL);
gst_bin_add_many(GST_BIN(pipeline), src, video_parse, myvpe, capsfilter1, enc, sink, NULL);
if (gst_element_link_many(src, video_parse, myvpe, capsfilter1, enc, sink) != TRUE)
{
g_printerr("Elements could not be linked.\n");
gst_object_unref(pipeline);
return -1;
}
ret = gst_element_set_state(pipeline, GST_STATE_PLAYING);
if (ret == GST_STATE_CHANGE_FAILURE) {
g_printerr("Unable to set the pipeline to the playing state.\n");
gst_object_unref(pipeline);
return -1;
}
bus = gst_element_get_bus(pipeline);
msg = gst_bus_timed_pop_filtered(bus, GST_CLOCK_TIME_NONE, GST_MESSAGE_ERROR | GST_MESSAGE_EOS);
if (msg != NULL)
gst_message_unref(msg);
gst_object_unref(bus);
gst_element_set_state(pipeline, GST_STATE_NULL);
gst_object_unref(pipeline);
return 0;
}
Then,I ran this code.It encountered a problem:
(gst-test:1185): GLib-GObject-CRITICAL **: g_object_unref: assertion 'G_IS_OBJECT (object)' failed
Elements could not be linked.
However,I use the same pipeline with command line successful:
gst-launch-1.0 filesrc location=/mnt/akiyo_qcif.yuv ! videoparse width=176 height=144 format=i420 ! videoconvert ! 'video/x-raw, format=(string)NV12, framerate=(fraction)25/1, width=(int)176, height=(int)144' ! ducatih264enc ! filesink location=x.h264
so,could you tell me how to deal with this problem.Thank you.