Part Number: TMS320C6678
Hi,
We use TI c6608 TI DSP. all 8 cores get an Hwi Interrupt at 1 ms each.But sometimes say once in 10000 times,Core id 0 receives interrupt with around 30000 cycles delay(25 micros),
this issue is not with other cores.None of the threads/interrupts are running(we commented and tried). (Core Id 0 has only some non critical operations like telnet to DSP etc for logging)
one more issue in same core 0, when we create some Timer based interrupts using Timer_start module ,say we want to invoke timer interrupt after 250 micros,but its triggered after like 280 micros.
this also happens sometimes..
..
timerParams.periodType=Timer_PeriodType_MICROSECS;
timerParams.runMode=Timer_RunMode_ONESHOT;
timerParams.startMode=Timer_StartMode_USER;
timerHandle=Timer_create(8+CoreId,x,&timerParams,&y);
..
can you please help us in this regard.
Thanks,
Thomas