Part Number: TMDXIDK5718
Other Parts Discussed in Thread: MATHLIB
Tool/software: Code Composer Studio
Hi
Im programming for the C66 DSP on the idk5718.
In order to use the mathlib I added the mathlib package (Project settings -> CS Genaral -> RTSC -> Products and Repositories).
Unfortunately the linker still issues error messages about unresolved symbols (all symbols from the mathlib).
I then added the mathlib library file to the linker file search path (see screenshot). Then it compiled without errors.
Why do I have to include the mathlib library manually when I already included the mathlib in the RTSC tab?
This should show my intention to really use it...
Used versions:
Code Composer Studio V7.1.0
PDK: V1.0.6
Mathlib: V3.1.1.0
XDCTools V3.32.1.22
Regards,
Markus