Part Number: AM5718
Sitara Family and Friends,
Our friends have some questions on AM5718 and would appreciate any guidance on connecting to a 5Mpixel CMOS sensor (such as AR0521) which only has a CSI2 interface with output format in raw RGB data. Although we have much more experience connecting up DaVinci devices to said CMOS sensor, it would be useful to know if anyone has done any similar work with AM5718 to a CMOS sensor like the AR0521?
Their proposal is as follows: still use the CSI2 interface to connect to the AR0521, and when raw data come in - that will be saved into frame buffers by DMA. Then they would code up the function to transfer color space from RGB to YUV by DSP, but since the raw data frame rate is 5M@30fps, this has to be completed without losing any frames.
All things considered (CPU speed, DSP, DMA, bandwidth of memory process and AM5718 architecture), does this seem plausible? Any other suggestions, such as reverse-flow using one of the video input ports/etc?
Comments are welcomed and appreciated.
TY,
CY