Part Number: AM5718
Other Parts Discussed in Thread: SYSBIOS
Tool/software: TI-RTOS
Hi,
In one of our project we have planned to use the TI processor AM5718, and as per the requirement we need to go for the Safety Critical certification.
It would be great if anyone provide us the inputs / clarity for the following doubts we are having in using the TI RTOS for this Safety Critical Applications
- Is TI RTOS, SysBIOS is certified / compliance to DO178, if not is there any reference available for usage of TI RTOS in Safety Critical Applications so that we can claim that this RTOS is well proven and widely used in defence/avionics applications
- Does TI provides the complete source code of SysBIOS RTOS? if complete source code is not available can you please provide us the information on “for which all components of RTOS source code is available and for which it is not available”
- As our end application to be developed on AM5718 is an graphics SW, can you please provide us the information on source code availability on ‘Graphics SW Stack’ provided by TI like omapdrm/omapdss/SGX KM/supported graphics libraries (OpenGLES/libdrm/libdrm omap/SGX UM) etc…
- Is any other DO178B compliant RTOS like VxWorks/GreenHills Integrity is proven/available for AM5718.
- Whether TI provides Bare metal support for Cortex A15 processor module of AM5718
- For Graphics SW which is the suggested OS (TI RTOS / Linux / Bare Metal) on Cortex A15 processor