This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Windows Embedded Compact 7 and omap3530

Other Parts Discussed in Thread: OMAP3530

Good day!

I build image of Windows Embedded Compact 7 for omap3530, but i have a problem

when i boot image i've got message:


-----------------------------------------------------------
[0]: Address=0x84001000 Length=0x02e3350c Save=0x80001000
-----------------------------------------------------------
Download file type: 1
rom_offset=0x0.
ImageStart = 0x84001000, ImageLength = 0x2e3350c, LaunchAddr = 0x8400cce0

Completed file(s):
-------------------------------------------------------------------------------
[0]: Address=0x84001000 Length=0x2e3350c Name="" Target=RAM
ROMHDR at Address 84001044h
Launch Windows CE image by jumping to 0x8000cce0...

Windows CE Kernel for ARM (Thumb Enabled)
--- High Performance Frequecy is 32768 khz---

 

and than system hold up and nothing happends. Somebody has solved a problem? Anybody can help me?