This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6657: DDR PHY Calc v11.xlsx for 36-bit on C665x

Guru* 84110 points
Part Number: TMS320C6657

In the DDR PHY Calc spreadsheet, there is a comment in the Notes tab that v11.0 adds a tab for C6657, but there is not a tab for it. Is there a newer spreadsheet that does include that tab? Or for the C6657 configuration for 36-bit?

The last block of *_SLAVE_RATIO values on the PHY CALC tab specifically says "Not valid for C665x".

Which registers should be used and which values when using the C6657 with ECC?

Regards,
RandyP