This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320DM8168: TMS320DM8168 Processor is Hanging while streaming video

Part Number: TMS320DM8168


Hello All,

We have designed a custom board based on DM8168 processor. The issue is when i run the gst pipeline for streaming or capturing the video the board is get hanging. Hardware point of view we have verified all power, reset , clocks and all looks fine, even when the board hangs all power,clock,resets are stable.  Is there anything to check on DDR3 ?  We are using micron DDR3 part MT41K128M16JT-125 and is already verified in the old production batch. We are seeing this issue on newly assembled boards , is this because of DSP core?  Any suggestions? 

And i have read the old thread and the issue looks similar to what we are seeing(below is the thread), is that solved? any updates from the user?

http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/p/437079/2211341#2211341

Below is the gst pipeline we are using to stream video:
gst-launch-0.10 omx_camera input-interface=VIP1_PORTA capture-mode=SC_NON_MUX override-colorspace=false vif-mode=16BIT !video/x-raw-yuv,format=\(fourcc\)NV12,framerate=\(fraction\)50/1,width=\(int\)1280,height=\(int\)720! gstperf ! omx_h264enc profile=8 input-buffers=2 output-buffers=2 ! queue ! rtph264pay ! udpsink host=192.168.13.35 ttl-mc=32 port=5004
Please let us know your valuable comments on this, 
Thanks&Regards,
Shyamsundar