Hello,
My customer has a question about OSCVSS connection. They are connecting xtal under data sheet recommendation. Please take a look at Figure 6-6. On-Chip 1.2V Oscillator in the data sheet:
They examined several noise tests and in some case they found DSP sometimes hang up. They investigated into the issue and found a workaround; connecting OSCVSS to PCB ground.
Actually, this is not allowed in the data sheet. It says:
When an external crystal is used, oscillator (OSC_VSS, RTC_VSS) ground must be kept separate from other grounds and connected directly to the crystal load capacitor ground. These pins are shorted to VSS on the device itself and should not be connected to VSS on the circuit board. If a crystal is not used and the clock input is driven directly, then the oscillator VSS may be connected to board ground.
They have confirmed the workaround works in their use case, but because of data sheet statements, they has not decided yet to go with it...
I believe you must have some reasons not to connect OSCVSS to GND for proper device operation. Do you have any comments on this ?
Best Regards,
Naoki