Part Number: AM4372
Hello.
I have a question about the schematics of AM437x EVM.
May I use the same VTT termination resistor value on DDR_CLKx and other lines?
TRM specifies Zo as 50 ohm +/- 5ohm.
But I am curious why SK/EVM is put different resistor value.(DDR_CLKx are 49.9ohm, others are 47ohm)
Our target board is instable to read/write to/from DDR3.
I would like to clarify if we should follow EVM schematic. (47ohm and 49.9ohm)
Or, should follow TRM?.(50ohm +/-5ohm)
Best regards, RY