Other Parts Discussed in Thread: TMS320C6748, , ADS4245
Hi, ALL
Now we will ready to measure DSP performance with high speed data converter.
DSP:
TMS320C6748
TMS320C6657
AD converter criteria:
1) resolution:12-14bit
2) sampling rate: 80Msps
3) channel:1ch-4ch
4) interface : parallel or serial
(any device is available if this specification is satisfied with )
Target device:ADS4245
-interface : LVDS
So, which EVM should I select?
The series of C6k cannot interface with LVDS.
So, it seems ideal condition as below:
ADS4245EVM--LVDS--FPGA board---PCIe/SRIO---C6657
Is there any combination like A/D board with a TSW140x data capture card?
If not, should we select K2L with JESD204B data converter?
Best regards,
Kyt