Other Parts Discussed in Thread: CCSTUDIO, SYSBIOS
Tool/software: TI-RTOS
Hi,
I am trying to compile mcasp example using pdksetupenv.bat and pdkProjectCreate.bat files, But while creating project facing an error . Please help me to resolve this issue
I have installed CCS version as : 5.3.0.00090
=========================================================================
Configuration:
SOC : OMAPL137
BOARD : all
ENDIAN : little
MODULE : mcasp
PROCESSOR : dsp
PDK_SHORT_NAME : C:\ti\PDK_OM~1\packages\
=========================================================================
Checking Configuration...
Complete
=========================================================================
GGR
C:/ti
PDK_PARTNO : OMAPL137
PDK_ECLIPSE_ID : com.ti.pdk.omapl137
RTSC_PLATFORM_NAME : ti.platforms.evmOMAPL137
RTSC_TARGET : ti.targets.elf.C674
CCS_DEVICE : "com.ti.ccstudio.deviceModel.C6000.GenericC674xDevice"
*****************************************************************************
Detecting all projects in PDK and importing them in the workspace C:\ti\PDK_OM~1\packages\\MyExampleProjects
Detected Test Project: MCASP_Audio_evmOMAPL137_c674xExampleProject
--------------------------------------------------------------------------------
Creating project 'MCASP_Audio_evmOMAPL137_c674xExampleProject'...
!ERROR: Unknown RTSC product-type ID 'com.ti.pdk.omapl137'!
NOTE: Refer to the following list of available RTSC product-type IDs (the display-names in square brackets are for reference only):
ti.mas.dsplib.c674x [DSPLIB C674x]
com.ti.sdo.edma3 [EDMA3 Low Level Driver]
com.ti.rtsc.IPC [Inter-processor Communication]
com.ti.rtsc.SYSBIOS [SYS/BIOS]
com.ti.uia [System Analyzer (UIA Target)]
com.ti.rtsc.XDAIS [XDAIS]
com.ti.pdk.k2g [k2g PDK]
Copying macros.ini
The system cannot find the path specified.
0 file(s) copied.
No projects detected
Project generation complete
*****************************************************************************