Hello all,
I want to do some flash frogram in C6713DSK, Kindly give some procedure to do the flash program..
Thanks in advance
Shan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello all,
I want to do some flash frogram in C6713DSK, Kindly give some procedure to do the flash program..
Thanks in advance
Shan
Hai Mariana,
Thanks a lot for your valuable reply , I have done the flash program from the example file, But white i creating a new project for the flash program i am facing a problem on creating the .hex file, Please give me some steps to create a .hex file
once again thanks,
The steps are in the page I sent:
10) Use hex6x to create an hex file, use a example of cmd file – tells hex6x how to convert from .out to .hex. You can use a .cmd file to pass the options to the hex6x utility. You can edit the file at C:\Program Files\SoftwareDesignSolutions\FlashBurnDSK\examples\DSK6713\BlinkDSK6713\BlinkDSK6713_ahex.cmd for your application (maybe copy it to the same location as your project's map file).
a) In Windowns, go to Start->Run, type cmd.
b) Type (replace the path below with the path for the .cmd file for your application if needed):
C:\CCStudio_v3.1\c6000\cgtools\bin\hex6x C:\Program Files\SoftwareDesignSolutions\FlashBurnDSK\examples\DSK6713\BlinkDSK6713\BlinkDSK6713_ahex.cmd
c) A .hex file will be generated.