Part Number: TMS320C6657
Can you point me, please, to a GEL or C test that will help us validate that the 36-bit ECC interface is working correctly? A customer has managed to setup the DDR3 so it is functionally working, but it does not see easy to figure out a way to generate an ECC error to validate correction and detection and interrupts and status bits.
I found a reference to one for Keystone 2 in MCSDK UG Chapter Exploring, but that appears to work from U-boot and therefore from the ARM in K2, but we are working with K1 C6657.
Regards,
RandyP