Part Number: PROCESSOR-SDK-K2G
Tool/software: TI-RTOS
processor_sdk_rtos_k2g_4_00_00_04
pdk_k2g_1_0_6
I got error when building custom board library with output files generated from TI PinMux.
According to SDK RTOS Release Notes of processor_sdk_rtos_k2g_4_00_00_04,
"Pinmux Tool Integration to Board Library for K2GEVM,K2GICE and AM571x IDK"
I added PR0_PRU0 GPIs and GPOs by selecting PRU_ICSS0_PRU under "Peripherals" tab in TI PinMux tool v4.0.1492. See the figure below.
The generated output file, 66AK2G0x_pinmux_data.c, contains the following:
...
#ifndef BUILDCFG_MOD_PRU_ICSS
#define BUILDCFG_MOD_PRU_ICSS
#endif /* BUILDCFG_MOD_PRU_ICSS */
...
#if defined(BUILDCFG_MOD_PRU_ICSS)
{CHIPDB_MOD_ID_PRU_ICSS, gPru_icssPinCfg},
#endif /* if defined(BUILDCFG_MOD_PRU_ICSS) */
...
But when built board library I got "CHIPDB_MOD_ID_PRU_ICSS" undefined error as followed:
...
"src/evmK2G/66AK2G0x_pinmux_data.c", line 2132: error #20: identifier
"CHIPDB_MOD_ID_PRU_ICSS" is undefined
1 error detected in the compilation of "src/evmK2G/66AK2G0x_pinmux_data.c".
...
It seems the PRU module is missing in the header file, pinmux.h.
C:\ti\pdk_k2g_1_0_6\packages\ti\board\src\evmK2G\include\pinmux.h
typedef enum
{
CHIPDB_MOD_ID_CPTS,
CHIPDB_MOD_ID_PWMSS,
CHIPDB_MOD_ID_MCASP,
CHIPDB_MOD_ID_DSS,
CHIPDB_MOD_ID_TIMER,
CHIPDB_MOD_ID_DCAN,
CHIPDB_MOD_ID_GPIO,
CHIPDB_MOD_ID_MCBSP,
CHIPDB_MOD_ID_UART,
CHIPDB_MOD_ID_PCIE,
CHIPDB_MOD_ID_MMCSD,
CHIPDB_MOD_ID_DEBUGSS,
CHIPDB_MOD_ID_GPMC,
CHIPDB_MOD_ID_EMAC,
CHIPDB_MOD_ID_CPSW,
CHIPDB_MOD_ID_DDR,
CHIPDB_MOD_ID_MCSPI,
CHIPDB_MOD_ID_USB,
CHIPDB_MOD_ID_SYSTEM,
CHIPDB_MOD_ID_I2C,
CHIPDB_MOD_ID_QSPI,
CHIPDB_MOD_ID_MLB,
CHIPDB_MOD_ID_INVALID = UINT32_MAX
} chipdbModuleID_t;
I can build my custom board library successfully after added "CHIPDB_MOD_ID_PRU_ICSS" in pinmux.h.
Is this the correct way to build board library? Am I missing anything else? Thanks.