This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: GPIO power supply

Part Number: AM5728

Hi,

For example, GPIO2 has the following power block.
I think that the used voltage of VDDSHV is different and the power supply to use may be different within GPIO2.
Is there a problem with this usage?

******************
GPIO2-1
~        VDDSHV10(1.8V)
GPIO2-8
******************
GPIO2-9
~        VDDSHV11(3.3V)
GPIO2-18
******************
GPIO2-19
~        VDDSHV10(1.8V)
GPIO2-28
******************
GPIO2-29     VDDSHV3(3.3V)
******************
GPIO2-30
GPIO2-31     VDDSHV6(3.3V)
******************

Best Regards,
Shigehiro Tsuda