Part Number: AM3354
Hi,
I m working on a custom board using AM3354 and connected a 800X400 24RGB interface LCD. Had set the LCD parameters as provided in the datasheet and found mismatch in the waveforms (Timings) compared with calculation.
Attached the calculation - LCD_Timing_Calcaultions_1.xlsx
i have Highlighted the cells which seems to be wrong- back porch values. is there any setting need to be done to match the waveforms and timings as per the calculations?
Below waveforms for HSD value 48.
Channel 1: Clock,
Channel 2: Data Enable:
Channel 3: HSD
Channel 4: VSD
HSD Back Porch-
VSD back porch-
Regards
Sujay A