Other Parts Discussed in Thread: TVP7002
I'm using dm6467T and dvsdk is 3.1 version. If I use a dvd-player as a video source, the encodedecode demo runs well. However, if i use a CCD camera as a video source, then there is an error:
root@dm6467t-evm:/mnt/dvsdk/dm6467# ./encodedecode
Encodedecode demo started.
vpif_capture vpif_capture: Error getting the standard info
Error: Failed to create capture device, 720P component input connected?
Both of the two video sources are 720p.