This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/OMAP5432-EVM-EVAL-SW: need to boot Android

Part Number: OMAP5432-EVM-EVAL-SW

Tool/software: Linux

Dear all,

 I tried booting Android to OMAP5432 when i connect USB And USB3 to my host system via HUB and opened terminal (screen @115200 baud-rate) but i am not getting any information about Device (Boot Switch position "0000") is this any issue with H/W


I refereed "omapedia.org/wiki/Panda5AJ.1.5_Release_Notes#"

Regards,

Hussain

  • Hi,

    The referred wiki is the correct one. I've successfully booted Android on the OMAP5 uEVM using these steps .
    Did you successfully executed all the steps listed in omapedia.org/wiki/Panda5AJ.1.5_Release_Notes ?
    For the debug console you need to connect the DEBUG USB. You need the USB3.0 Port only for flashing the device.

    Best Regards,
    Yordan