This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux: Gadget Device. Problem loading module g_ether.ko

Other Parts Discussed in Thread: OMAP-L138

Tool/software: Linux

Hi,
I'm trying to use a gadget device, for example, ethernet or hid.

When I load the module with:

modprobe g_ether

with the command dmesg I see the error:

udc-core: could not find an available UDC - added [g_ether] to list of pending drivers

and the gadget device does not work.

I am using the SDK:

PROCESSOR-SDK-LINUX-OMAPL138 04_00_00_04

I work with the target:
OMAP-L138 DSP + ARM9 Development Kit (LCDK)

Someone has a gadget device running and could you help me?

Thank you.

Antonio