This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/DRA726: How to set PWM in u-boot on DRA726

Part Number: DRA726

Tool/software: Linux

I have implemented the splash screen on our DRA726 board, I load an image from QSPI during u-boot and load the linux kernel. The picture will appear on the screen about 6-7 seconds later.

The reason is that the backlight is not on until the backlight driver on linux turns the backlight on. I need help on getting the pwm on. It could be acceptable to have it at 100% but preferable if it was configurable.

There is no pwm driver in u-boot. I looked at the linux driver but it is not obvious if or how that could be ported to u-boot.

Here is the entry in the linux devicetree, a gpio is used to turn the output on and ehrpwm1A (G6) is used to set the backlight duty cycle.

        lcd_bl: backlight {                                                                                      
                compatible = "pwm-backlight";                                                                    
                pwms = <&ehrpwm0 0 50000 0>;                                                                     
                                                                                                                 
                brightness-levels =                                                                              
                        <0  1  2  3  4  5  6  7  8  9 10 11 12 13 14 15 16 17 18 19                              
                        20 21 22 23 24 25 26 27 28 29 30 31 32 33 34 35 36 37 38 39                              
                enable-gpios = <&gpio6 6 GPIO_ACTIVE_HIGH>;                                                      
                                                                                                                 
                /* 0 to 255 */                                                                                   
                        40 41 42 43 44 45 46 47 48 49 50 51 52 53 54 55 56 57 58 59                              
                        60 61 62 63 64 65 66 67 68 69 70 71 72 73 74 75 76 77 78 79                              
                        80 81 82 83 84 85 86 87 88 89 90 91 92 93 94 95 96 97 98 99                              
                        100 101 102 103 104 105 106 107 108 109 110 111 112 113 114 115 116 117 118 119          
                        120 121 122 123 124 125 126 127 128 129 130 131 132 133 134 135 136 137 138 139          
                        140 141 142 143 144 145 146 147 148 149 150 151 152 153 154 155 156 157 158 159          
                        160 161 162 163 164 165 166 167 168 169 170 171 172 173 174 175 176 177 178 179          
                        180 181 182 183 184 185 186 187 188 189 190 191 192 193 194 195 196 197 198 199          
                        200 201 202 203 204 205 206 207 208 209 210 211 212 213 214 215 216 217 218 219          
                        220 221 222 223 224 225 226 227 228 229 230 231 233 232 234 234 236 237 238 239          
                        240 241 242 243 244 245 246 247 248 249 250 251 252 253 254 255>;                        
                                                                                                                 
                default-brightness-level = <127>;                                                                
        };                                                                                                       

Michel Catudal

ACTIA Corp