Part Number: AM3894
Tool/software: Linux
Hi all,
My code base is EZSDK_5_04_00_11 and use custom AM3894 (silicon revision 2.1) board.
I want to configure USB0 module to slave mode. Here are my queries.
1. How to handle USB0_DRVVBUS (P35) pin?
Just add a pull high 10K resistor to 3.3V or not.
2. Does select a GPIO pin to connect with USB connector ID pin as floating state?
Thanks in advance.
B.R.
OC