This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

fvid_creat problem



dear all
Rencently,I create a project to realize video sample and h.264 encode and decode. So I

build a project upon the example given by ti, named video_encdec,however,I found there is a

problem,when I debug My programm, it stops at
 CcdcHandle              = FVID_create("/VPFE0",IOM_INOUT,NULL,&feinitParams,&gioAttrs);
I create this handle with follow steps,
1 in the .tcf file,I wrote :
bios.UDEV.create("VPFE0");
bios.UDEV.instance("VPFE0").fxnTableType = "IOM_Fxns";
bios.UDEV.instance("VPFE0").fxnTable = prog.extern("VPFEMD_FXNS");
2,in the program,
feinitParams.id         = PSP_VPFE_CCDC;
    feinitParams.params     = (PSP_VPFECcdcConfigParams*)&ccdcParams;
    CcdcHandle              = FVID_create("/VPFE0",IOM_INOUT,NULL,&feinitParams,&gioAttrs);
    if(NULL == CcdcHandle)
    {
      
        return;
    }
when I click run the program, there is no reponse,so I step into this program,I find when

it go to a function named hwi_disable1,and then it jump back,and ccdchandle=0,I don't know

what's the problem.
by the way,there is another problem,when I click debug->go main,it doesn't go to the main

funciton,it seems there is no response,but when i click stop,from the disassembly windown,i

can see it always stops at hwi15+addr.
 some times,if I click go main for several times,it jumps out a message box:can't set a

breakpoint to gel_go()(almost this mean),I am puzzeled by these problem,I am waiting for

your help,thanks.