I am using Spectrum Digital's DM365 EVM and DVSDK version 3.10. From my looking around it appears that making use of the DMAI package in the DVSDK would be the best approach for us in the long run. However, I'm getting confused as to how to set up the Capture module in the DMAI package for our application.
We are connecting a camera to the camera interface connector (J10) on the DM365 EVM. The camera is outputting 5 MP raw Bayer formatted images. Overall the setup to use the Capture module to receive video seems simple, the Capture module allows for composite, component, or s-video video input types (Capture_Attrs.videoInput). What do I do in the case of raw Bayer input on J10?
Are there any examples that come with the DVSDK 3.10 that use J10 as the video input?
Thanks,
Bryan