Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: AM3352
We have a custom board based on am3352 with Micrel KSZ9031 Gigabit PHY.
Single PHY on EMAC1, phy_id=3.
Linux configuration and device-tree is derived from TI am3355x-evm.
The Linux build is using ti-processor-sdk-linux-am335x-evm-04.00.00.04.
This is about the 13-th SDK version we use and so far the Ethernet has
always worked fine at 100/1000 Mbit.
Now the kernel seems not to recognize Micrel PHY.
[ 1.172821] 0x000000000000-0x000000200000 : "SPIFLASH.file-system"
[ 1.181715] libphy: Fixed MDIO Bus: probed
[ 1.255300] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
[ 1.261696] davinci_mdio 4a101000.mdio: detected phy mask fffffff7
[ 1.269205] libphy: 4a101000.mdio: probed
[ 1.273418] davinci_mdio 4a101000.mdio: phy[3]: device
4a101000.mdio:03, driver Micrel KSZ9031 Gigabit PHY
[ 16.317829] net eth0: initializing cpsw version 1.12 (0)
[ 16.323419] net eth0: initialized cpsw ale version 1.4
[ 16.391354] net eth0: ALE Table size 1024
[ 16.517942] Micrel KSZ9031 Gigabit PHY 4a101000.mdio:03: attached PHY
driver [Micrel KSZ9031 Gigabit PHY] (mii_bus:phy_addr=4a101000.mdio:03,
irq=-1)
[ 16.589384] libphy: PHY not found
[ 16.592972] net eth0: phy "" not found on slave 1, err -19
[ 16.645168] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 18.646573] cpsw 4a100000.ethernet eth0: Link is Up - 100Mbps/Full -
flow control rx/tx
[ 18.655043] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
The phenomenom is similar to what is reported on the forum
Have not checked the Ethernet behavior from u-boot, because for us this
is not important.
Attachments:
bootlog.txt
Network report log (ifconfig and ethtool)
Board device-tree
Linux configuration
Diff of Linux config with respect to TI am335x-evm
Looking forward to solution and/or suggestions to remedy the problem.
Best regardsKSZ9031.zip