Part Number: TDA2EVM5777
Other Parts Discussed in Thread: TDA2
Tool/software: Linux
Hello!
I've got a problem using linux on DRA7xxx (XC5777X Board):
The "remoteproc" is not usable in SDK "Vision_SDK_2_12_02_00".
The Kernel used in this SDK is a special patched linux-4.4.45 without generating the "sys/class/remoteproc" - control stuff!
The mainline Kernel 4.13.0 is far away from the kernel used in the SDK, so backporting will not be as easy... but remoteproc is fully integrated.
(Without any kind of TDA2 ipu or dsp support...? At least I can not not find any usable dts-file, or any supporting code... )
Do you have a newer linux kernel than 4.4 dealing with TDA2 subcores and fully suppored remoteproc?
I have to work with M4 and DSP in TDA2 bare metal, so controlling the subcores with remoteproc (start, stop, etc...) is needed.
Thank you... Marco.