This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM3352: Is AM335x SDK6.0 Support IPV6 or not?

Part Number: AM3352

Tool/software: Linux

Hi Experts,

Processor: AM335x
SDK: TI SDK 6.0

I know SDK 6.0 is really old SDK versiuon and TI may not maintain anymore.
But our customer is facing an issue for adding IPV6 function in their product.
While customer add IPV6 function in SDK 6.0, it show up the following log: (Attachment is dmesg log file, FYR)

[    0.000000] Linux version 3.2.0 (saho@ubuntu) (gcc version 4.7.3 20130226 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013.03) ) #1 Fri Jun 17 09:25:32 CST 2016
[    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] Machine: am335xevm
[    0.000000] Memory policy: ECC disabled, Data cache writeback
[    0.000000] On node 0 totalpages: 65536
[    0.000000] free_area_init_node: node 0, pgdat c06cbde8, node_mem_map c0706000
[    0.000000]   Normal zone: 512 pages used for memmap
[    0.000000]   Normal zone: 0 pages reserved
[    0.000000]   Normal zone: 65024 pages, LIFO batch:15
[    0.000000] AM335X ES2.1 (neon )
[    0.000000] pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
[    0.000000] pcpu-alloc: [0] 0 
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 65024
[    0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 ro rootfstype=ext3 rootwait ip=none
[    0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[    0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[    0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[    0.000000] Memory: 256MB = 256MB total
[    0.000000] Memory: 252664k/252664k available, 9480k reserved, 0K highmem
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
[    0.000000]     vmalloc : 0xd0800000 - 0xff000000   ( 744 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xd0000000   ( 256 MB)
[    0.000000]     modules : 0xbf000000 - 0xc0000000   (  16 MB)
[    0.000000]       .text : 0xc0008000 - 0xc060b000   (6156 kB)
[    0.000000]       .init : 0xc060b000 - 0xc0667000   ( 368 kB)
[    0.000000]       .data : 0xc0668000 - 0xc06d57d0   ( 438 kB)
[    0.000000]        .bss : 0xc06d57f4 - 0xc0705a28   ( 193 kB)
[    0.000000] NR_IRQS:396
[    0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[    0.000000] Total of 128 interrupts on 1 active controller
[    0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz
[    0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz
[    0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
[    0.000000] Console: colour dummy device 80x30
[    0.000091] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736)
[    0.089233] pid_max: default: 32768 minimum: 301
[    0.089355] Security Framework initialized
[    0.089447] Mount-cache hash table entries: 512
[    0.089813] CPU: Testing write buffer coherency: ok
[    0.109344] omap_hwmod: gfx: failed to hardreset
[    0.125122] omap_hwmod: pruss: failed to hardreset
[    0.126159] print_constraints: dummy: 
[    0.126495] NET: Registered protocol family 16
[    0.128326] OMAP GPIO hardware version 0.1
[    0.130493] omap_mux_init: Add partition: #1: core, flags: 0
[    0.132171]  omap_i2c.1: alias fck already exists
[    0.132934]  omap2_mcspi.1: alias fck already exists
[    0.133087]  omap2_mcspi.2: alias fck already exists
[    0.133850]  edma.0: alias fck already exists
[    0.133880]  edma.0: alias fck already exists
[    0.133880]  edma.0: alias fck already exists
[    0.155151] bio: create slab <bio-0> at 0
[    0.157012] SCSI subsystem initialized
[    0.158386] usbcore: registered new interface driver usbfs
[    0.158660] usbcore: registered new interface driver hub
[    0.158813] usbcore: registered new device driver usb
[    0.159088] registerd cppi-dma Intr @ IRQ 17
[    0.159118] Cppi41 Init Done Qmgr-base(d087a000) dma-base(d0878000)
[    0.159118] Cppi41 Init Done
[    0.159149] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3
[    0.159454] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1
[    0.160400] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz
[    0.162109] tps65910 1-002d: JTAGREVNUM 0x0
[    0.164398] print_constraints: VRTC: 
[    0.165802] print_constraints: VIO: at 1500 mV 
[    0.168029] print_constraints: VDD1: 600 <--> 1500 mV at 1325 mV normal 
[    0.170257] print_constraints: VDD2: 600 <--> 1500 mV at 1137 mV normal 
[    0.171203] print_constraints: VDD3: 5000 mV 
[    0.172515] print_constraints: VDIG1: at 1800 mV 
[    0.173889] print_constraints: VDIG2: at 1800 mV 
[    0.175231] print_constraints: VPLL: at 1800 mV 
[    0.176605] print_constraints: VDAC: at 1800 mV 
[    0.177947] print_constraints: VAUX1: at 1800 mV 
[    0.179321] print_constraints: VAUX2: at 3300 mV 
[    0.180664] print_constraints: VAUX33: at 3300 mV 
[    0.182037] print_constraints: VMMC: at 3300 mV 
[    0.182434] tps65910 1-002d: No interrupt support, no core IRQ
[    0.183563] Advanced Linux Sound Architecture Driver Version 1.0.24.
[    0.184539] Switching to clocksource gp timer
[    0.196319] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[    0.196533] musb-hdrc musb-hdrc.0: dma type: dma-cppi41
[    0.196807] MUSB0 controller's USBSS revision = 4ea20800
[    0.196838] TxFifo Empty intr disabled
[    0.196838] musb0: Enabled SW babble control
[    0.197113] musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
[    0.197143] musb-hdrc: MHDRC RTL version 2.0 
[    0.197143] musb-hdrc: setup fifo_mode 4
[    0.197174] musb-hdrc: 28/31 max ep, 16384/16384 memory
[    0.197174] musb-hdrc.0: bulk split disabled
[    0.197204] musb-hdrc.0: bulk combine disabled
[    0.197662] musb-hdrc musb-hdrc.0: USB OTG mode controller at d083c000 using DMA, IRQ 18
[    0.197814] musb-hdrc musb-hdrc.1: dma type: dma-cppi41
[    0.198089] MUSB1 controller's USBSS revision = 4ea20800
[    0.198120] TxFifo Empty intr disabled
[    0.198120] musb1: Enabled SW babble control
[    0.198394] musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
[    0.198394] musb-hdrc: MHDRC RTL version 2.0 
[    0.198394] musb-hdrc: setup fifo_mode 4
[    0.198425] musb-hdrc: 28/31 max ep, 16384/16384 memory
[    0.198425] musb-hdrc.1: bulk split disabled
[    0.198425] musb-hdrc.1: bulk combine disabled
[    0.198486] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[    0.198577] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1
[    0.198699] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[    0.198699] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    0.198730] usb usb1: Product: MUSB HDRC host driver
[    0.198730] usb usb1: Manufacturer: Linux 3.2.0 musb-hcd
[    0.198730] usb usb1: SerialNumber: musb-hdrc.1
[    0.199432] hub 1-0:1.0: USB hub found
[    0.199462] hub 1-0:1.0: 1 port detected
[    0.199890] musb-hdrc musb-hdrc.1: USB Host mode controller at d083e800 using DMA, IRQ 19
[    0.200256] NET: Registered protocol family 2
[    0.200439] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
[    0.200805] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
[    0.200927] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
[    0.200988] TCP: Hash tables configured (established 8192 bind 8192)
[    0.200988] TCP reno registered
[    0.201019] UDP hash table entries: 256 (order: 0, 4096 bytes)
[    0.201019] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[    0.201202] NET: Registered protocol family 1
[    0.201416] RPC: Registered named UNIX socket transport module.
[    0.201446] RPC: Registered udp transport module.
[    0.201446] RPC: Registered tcp transport module.
[    0.201446] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.201660] NetWinder Floating Point Emulator V0.97 (double precision)
[    0.212951] VFS: Disk quotas dquot_6.5.2
[    0.213012] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[    0.213470] msgmni has been set to 493
[    0.216308] alg: No test for stdrng (krng)
[    0.216979] io scheduler noop registered
[    0.216979] io scheduler deadline registered
[    0.217041] io scheduler cfq registered (default)
[    0.218109] Could not set LED4 to fully on
[    0.255584] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[    0.910949] console [ttyO0] enabled
[    0.915161] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[    0.922912] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[    0.930664] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[    0.938385] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[    0.946105] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[    0.954223] omap4_rng omap4_rng: OMAP4 Random Number Generator ver. 2.00
[    0.968475] brd: module loaded
[    0.975524] loop: module loaded
[    0.978973] i2c-core: driver [tsl2550] using legacy suspend method
[    0.985473] i2c-core: driver [tsl2550] using legacy resume method
[    0.991882] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[    1.075164] No daughter card found
[    1.078765] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[    1.086059] Setup board 1
[    1.088775] Setup board 2
[    1.091522] Setup board 3
[    1.094238] Setup board 4
[    1.096984] Board name: A335X_SK
[    1.100341] Board version: 
[    1.103271] The board is a AM335x Starter Kit.
[    1.107910] [BOARD]:bq32k_init() 
[    1.111389] i2c i2c-1: Failed to register i2c client rtc-bq32k at 0x68 (-16)
[    1.118774] failed to register lis331dlh to i2c1
[    1.123870]  omap_hsmmc.1: alias fck already exists
[    1.129180] usb 1-1: new high-speed USB device number 2 using musb-hdrc
[    1.136505]  omap_hsmmc.0: alias fck already exists
[    1.142364]  da8xx_lcdc.0: alias fck already exists
[    1.147888] da8xx_lcdc da8xx_lcdc.0: GLCD: Found NHD-4.3-ATXI#-T-1 panel
[    1.163116] Console: switching to colour frame buffer device 60x34
[    1.175720]  davinci-mcasp.0: alias fck already exists
[    1.181549] [BOARD] Saho_gpio_init 
[    1.185302] _omap_mux_get_by_name: Could not find signal uart1_rtsn.	gpio0_13
[    1.192962] _omap_mux_get_by_name: Could not find signal gpmc-wpn.gpio0_31
[    1.208404] registered am33xx_sr device
[    1.214080] mtdoops: mtd device (mtddev=name/number) must be supplied
[    1.221221] omap2-nand driver initializing
[    1.225677] OneNAND driver initializing
[    1.230743] CAN device driver interface
[    1.234741] CAN bus driver for Bosch D_CAN controller 1.0
[    1.276489] usb 1-1: New USB device found, idVendor=05e3, idProduct=0610
[    1.283508] usb 1-1: New USB device strings: Mfr=0, Product=1, SerialNumber=0
[    1.290985] usb 1-1: Product: USB2.0 Hub
[    1.295349] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
[    1.301818] davinci_mdio davinci_mdio.0: detected phy mask fffffffe
[    1.309600] davinci_mdio.0: probed
[    1.313171] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown
[    1.320739] hub 1-1:1.0: USB hub found
[    1.324768] PPP generic driver version 2.4.2
[    1.329376] hub 1-1:1.0: 4 ports detected
[    1.333892] PPP Deflate Compression module registered
[    1.339569] usbcore: registered new interface driver zd1201
[    1.345672] usbcore: registered new interface driver cdc_ether
[    1.351959] usbcore: registered new interface driver cdc_eem
[    1.358123] usbcore: registered new interface driver dm9601
[    1.364013] cdc_ncm: 04-Aug-2011
[    1.367614] usbcore: registered new interface driver cdc_ncm
[    1.373901] usbcore: registered new interface driver cdc_acm
[    1.379852] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
[    1.388580] usbcore: registered new interface driver cdc_wdm
[    1.394500] Initializing USB Mass Storage driver...
[    1.399841] usbcore: registered new interface driver usb-storage
[    1.406158] USB Mass Storage support registered.
[    1.411285] usbcore: registered new interface driver usbserial
[    1.417510] USB Serial support registered for generic
[    1.422912] usbcore: registered new interface driver usbserial_generic
[    1.429779] usbserial: USB Serial Driver core
[    1.434417] USB Serial support registered for GSM modem (1-port)
[    1.440948] usbcore: registered new interface driver option
[    1.446807] option: v0.7.2:USB Driver for GSM modems
[    1.452087] USB Serial support registered for pl2303
[    1.457427] usbcore: registered new interface driver pl2303
[    1.463256] pl2303: Prolific PL2303 USB to serial adaptor driver
[    1.470031] mousedev: PS/2 mouse device common for all mice
[    1.479309] bq32k 1-0068: rtc core: registered bq32k as rtc0
[    1.485717] i2c /dev entries driver
[    1.489715] Linux video capture interface: v2.00
[    1.494842] usbcore: registered new interface driver uvcvideo
[    1.500854] USB Video Class driver (1.1.1)
[    1.646087] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[    1.654541] cpuidle: using governor ladder
[    1.659210] usb 1-1.1: new high-speed USB device number 3 using musb-hdrc
[    1.666534] cpuidle: using governor menu
[    1.674224] omap4_aes_mod_init: loading AM33X AES driver
[    1.679931] omap4-aes omap4-aes: AM33X AES hw accel rev: 3.02
[    1.686767] omap4_aes_probe: probe() done
[    1.691192] omap4_sham_mod_init: loading AM33X SHA/MD5 driver
[    1.697357] omap4-sham omap4-sham: AM33X SHA/MD5 hw accel rev: 4.03
[    1.711303] omap4_sham_probe: probe() done
[    1.721008] usbcore: registered new interface driver usbhid
[    1.726867] usbhid: USB HID core driver
[    1.731628] usbcore: registered new interface driver snd-usb-audio
[    1.739776] _regulator_get: 1-001b supply IOVDD not found, using dummy regulator
[    1.747589] _regulator_get: 1-001b supply DVDD not found, using dummy regulator
[    1.755310] _regulator_get: 1-001b supply AVDD not found, using dummy regulator
[    1.762969] _regulator_get: 1-001b supply DRVDD not found, using dummy regulator
[    1.773162] asoc: tlv320aic3x-hifi <-> davinci-mcasp.0 mapping ok
[    1.780792] ALSA device list:
[    1.783874]   #0: AM335X EVM
[    1.786926] oprofile: hardware counters not available
[    1.792205] oprofile: using timer interrupt.
[    1.796844] nf_conntrack version 0.5.0 (3947 buckets, 15788 max)
[    1.803497] ip_tables: (C) 2000-2006 Netfilter Core Team
[    1.809204] TCP cubic registered
[    1.812683] NET: Registered protocol family 10
[    1.818084] Mobile IPv6
[    1.820648] IPv6 over IPv4 tunneling driver
[    1.826568] NET: Registered protocol family 17
[    1.831268] can: controller area network core (rev 20090105 abi 8)
[    1.837890] NET: Registered protocol family 29
[    1.842529] can: raw protocol (rev 20090105)
[    1.847015] can: broadcast manager protocol (rev 20090105 t)
[    1.852966] Registering the dns_resolver key type
[    1.857940] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[    1.865966] ThumbEE CPU extension supported.
[    1.870513] mux: Failed to setup hwmod io irq -22
[    1.876068] Power Management for AM33XX family
[    1.880950] Trying to load am335x-pm-firmware.bin (60 secs timeout)
[    1.887664] Copied the M3 firmware to UMEM
[    1.892028] Cortex M3 Firmware Version = 0x181
[    1.896820] DIEID: 1002600d 016054cd 00000000 592c0002
[    1.896820] EFUSE SMA register val = 00013c2f
[    1.896850] Compensating OPP0: Orig nvalue:0x99bfac New nvalue:0x99bfac
[    1.896850] Compensating OPP1: Orig nvalue:0x9a8af8 New nvalue:0x9a8af8
[    1.898376] Compensating OPP0: Orig nvalue:0x99b9ac New nvalue:0x99b9ac
[    1.898376] Compensating OPP1: Orig nvalue:0x999486 New nvalue:0x999486
[    1.898406] Compensating OPP2: Orig nvalue:0xaae3ce New nvalue:0xaae3ce
[    1.898406] Compensating OPP3: Orig nvalue:0xaacbb8 New nvalue:0xaacbb8
[    1.898406] Compensating OPP4: Orig nvalue:0xaacbb8 New nvalue:0xaa9b8e
[    1.898498] create_regulator: VDD1: Failed to create debugfs directory
[    1.906860] smartreflex smartreflex: am33xx_sr_probe: Driver initialized
[    1.915618] usb 1-1.1: New USB device found, idVendor=0bda, idProduct=8179
[    1.922851] usb 1-1.1: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[    1.930480] usb 1-1.1: Product: 802.11n NIC
[    1.934875] usb 1-1.1: Manufacturer: Realtek
[    1.939331] usb 1-1.1: SerialNumber: 00E04C0001
[    1.950744] clock: disabling unused clocks to save power
[    1.959350] mmc0: new high speed MMC card at address 0001
[    1.965698] mmcblk0: mmc0:0001 SEM04G 3.68 GiB 
[    1.970825] mmcblk0boot0: mmc0:0001 SEM04G partition 1 2.00 MiB
[    1.977203] mmcblk0boot1: mmc0:0001 SEM04G partition 2 2.00 MiB
[    1.984954]  mmcblk0: p1 p2
[    1.990386]  mmcblk0boot1: unknown partition table
[    1.997283]  mmcblk0boot0: unknown partition table
[    2.008911] Detected MACID=1c:ba:8c:a5:89:fc
[    2.014678] cpsw: Detected MACID = 1c:ba:8c:a5:89:fe
[    2.022186] bq32k 1-0068: setting system clock to 2017-08-04 09:01:20 UTC (1501837280)
[    2.033325] EXT3-fs (mmcblk0p2): recovery required on readonly filesystem
[    2.040466] EXT3-fs (mmcblk0p2): write access will be enabled during recovery
[    2.169067] SR 0: curr=1137500, delta_v=-56875, calc=1080625, act=1087500, gain=00
[    2.172698] SR 1: curr=1325000, delta_v=-66250, calc=1258750, act=1262500, gain=00
[    2.418853] kjournald starting.  Commit interval 5 seconds
[    2.424652] EXT3-fs (mmcblk0p2): recovery complete
[    2.432312] EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode
[    2.439605] VFS: Mounted root (ext3 filesystem) readonly on device 179:2.
[    2.447204] Freeing init memory: 368K
[    3.421142] SR 0: curr=1087500, delta_v=-88864, calc=998636, act=1000000, gain=1b
[    3.430725] SR 1: curr=1262500, delta_v=36456, calc=1298956, act=1300000, gain=34
[    5.660705] EXT3-fs (mmcblk0p2): using internal journal
[    5.958801] SR 1: curr=1300000, delta_v=0, calc=1300000, act=1300000, gain=34
[    6.218811] net eth0: CPSW phy found : id is : 0x4dd074
[    6.231231] ADDRCONF(NETDEV_UP): eth0: link is not ready
[    7.828063] net eth0: CPSW phy found : id is : 0x4dd074
[    7.839202] ADDRCONF(NETDEV_UP): eth0: link is not ready
[    8.850585] SR 1: curr=1300000, delta_v=-5096, calc=1294904, act=1300000, gain=34
[    9.827606] PHY: 0:00 - Link is Up - 1000/Full
[    9.846923] ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[   14.366699] Loading kernel module for a network device with CAP_SYS_MODULE (deprecated).  Use CAP_NET_ADMIN and alias netdev- instead
[   20.076629] eth0: no IPv6 routers present
[   20.616607] eth0: no IPv6 routers present

Loading kernel module for a network device with CAP_SYS_MODULE (deprecated). Use CAP_NET_ADMIN and alias netdev- instead

My colleague told me that he remember SDK 6.0 is not support IPV6 function, but I can't fine any document or E2E thread told about it.

Here are my question:
1. Does TI SDK 6.0 support IPV6? If not, is there any document or E2E thread told abot it?
2. If TI SDK 6.0 support IPV6, is there any patch or user's guide customer can follow?

Best Regareds,
Wayne Kuo

  • Hello Wayne,

    By default ipv6 in SDK 6.0 is not enabled as in latest Processor SDK, ipv6 has support on Linux from a long time ago and AM335x does not have any restrictions with respect to it, it should be possible to make it work on SDK6.

    Best regards,
    Kemal