Part Number: AM4372
Other Parts Discussed in Thread: TPS65218
I have a new board design using the AM4372 and the recommended PMIC TPS65218. All the voltage rails are correct and the oscillator is running by the time the PORZ pin is released to high by the PMIC to start the CPU but on our boards (We have 3 prototypes) the CPU does not reliably start the ROM bootloader. The SYSBOOT boot pins are configured to boot from SDCARD and between 10 and 75% of the time the CPU will start correctly depending on which board we try.
Any guidance of where to look for problems would be appreciated.