This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Transcoding Using DM365.



Hello There:

Is there a way of doing video transcoding using the DM365?

Say that the input is an MPEG-2 video stream and the desired output is an H.264 video stream:

- Can the DM365 internally be able to transcode the video stream?

- Or can the DM365 decode the input stream and then encode it?

- Can you create different codec instances in the same code, even if they don't run at the same time?

Thank you.

Gabriel