Are there any specific configuration steps that must be taken to configure HyperLink for a single channel?
I am using CCSV7.1 with PDK_K2HK_4_0_4. I have the example application hyplnk_K2HC66DevLibBiosExample running on two EVMK2Hx development boards that are connected via a custom backplane. The example application executes successfully when executed with hyplnk_EXAMPLE_ALLOW_4_LANES defined but when this is not defined and I only have hyplnk_EXAMPLE_ALLOW_1_LANE defined then the application hangs on both boards. I have tried running the application with hyplnk_EXAMPLE_ALLOW_0_LANES defined and not defined. Neither case seems to make any difference. Are there other settings that need to be made to support a single channel configuration? I appears that there may be some low level initialization that relies on all four channels.
Thanks for your support,
Sincerely,
Jack